Vynckier Enclosure Systems

The World's Leading Manufacturer of Non-Metallic Enclosures

Toll Free: (888) 837-1114
New Extended Hours Monday - Friday 7:30am to 6pm CST

Vynckier Releases 20x16 JIC Enclosure: VJ2016

April 29, 2015


Vynckier Enclosure Systems broadens their JIC enclosure line to include the “extra depth” VJ2016, offering the industry’s deepest base.

The VJ2016 comes with 10.72” of usable depth, exceeding all of the standard or raised depth versions presently available in the market place of a 20x16 JIC enclosure.

A .197” wall thickness enhances the structural integrity of the enclosure wall, providing end users with the ability to house large, heavy components in the VJ2016.

The VJ2016 cover is mounted to the base using thru-holes and stainless steel hardware ensures corrosion resistance as well as the added strength.

Keeping true to the quality of Vynckier’s  VJ line, the new 20x16 enclosure includes the following features:

  • Full width mounting flange with added gusset strengtheners providing maximum static load capacity
  • Outdoor life exceeding 20 years (an additional 10 years if UV coated)
  • Optional cover printing for display of custom artwork (ie. company logo, product name, etc.)
  • Corner ribs on cover for added protection against cracks if dropped
  • Molded gasket channel housing memory retaining, poured, polyurethane gasket
  • Made in the USA


For more information or to find your local representative,
please visit our website at www.vynckier.com or call us directly at 1-888-837-1114

Author: Natalie Hart

“Out of the Box” Solution: Vynckier Enclosures DT Cover

August 28, 2012


Full Line of Inspection WindowsVynckier Enclosure Systems presents the perfect solution for external meters, monitors, and pushbuttons that need to be protected from the elements but are frequently accessed.

Exclusively available through Vynckier, the DT Cover Window Kit protects controls & instrumentation maintaining UL Type 4X integrity while still allowing operator access.

When ordered as a DT Cover KIT, even the novice installer can use this cover as it comes complete with mounting hardware and instructions.

The fiberglass (FRP) frame and clear Lexan window provide UL Type 4X protection in virtually any wet or corrosive environment, including:

  • Food Processing
  • Petro Chem
  • Pulp & Paper
  • Utility & Power Generation
  • Temporary Power Equipment & Drives
  • Mining Equipment
  • Asphalt/Cement Production
  • Exterior HVAC equipment
  • Hydraulic Equipment

The DT Cover window kit mounts on any flat surface, whether metal or non-metallic, and comes in 5 convenient sizes ranging from 12" x 7.5" to 12" x 24".

For more information or to find your local representative,
please visit our website at www.vynckier.com or call us directly at 713-374-7850

Author: Natalie Hart

Vynckier’s #1 Time Saving Offer: Modified Enclosures

September 20, 2012


Vynckier Enclosure Systems offers a comprehensive modification program to fit any project. We pride ourselves on the ability to repeatedly produce professional and accurate enclosure modifications every time.

We can customize your enclosures to your requirements and save your time and energy that would normally be spent doing so. Let us streamline your procedure by sending your enclosure complete with any holes, cut outs, windows, etc. that your specific job requires.

Vynckier’s professionally trained engineering staff coupled with state of the art design software and technologically advanced equipment produce perfect enclosure modifications of any size, shape and quantity.

  • Custom hole sizes and shapes
  • Custom cutout sizes and shapes
  • Custom window sizes and shapes
  • Vent, A/C, heater and air filter installation
  • Aluminum panel customization and threaded insert installation
  • Custom colors
  • Silk screening
  • EMI/RFI shielding

Send us a drawing or prototype and we will get our best pricing to you and help ensure your project is a success from budgetary stage to finished production.

Our machining capabilities allow quick turnaround, even at high quantities.

Once your enclosure is created according to your specifications, there is a quality control process before it ships to help provide turnkey service. Your product will ship fully assembled and ready to protect your product.

For more information or to find your local representative,
please visit our website at www.vynckier.com or call us directly at 713-374-7850

Vynckier: Conquering Obstacles for St. Jude

October 22, 2012


On October 6th, Vynckier Enclosure Systems competed, and crushed, a 5K race and obstacle course. Over 1600 dashers raced across the sand in support of St. Jude Children’s Research Hospital® on a course located on East Beach in Galveston, TX.

The course started out with about a 1 mile run that lead up to the first of ten grueling obstacles. The next 2 miles were broken up by ditches to trudge through, walls to scale, tunnels and quick sand. There were even flames to leap over before reaching the finish line.

Once the participants thought they could take no more, they were met at the finish line with live music and refreshments. The weather and after party were a perfect conclusion to such a strenuous afternoon.

The event was held in support of St. Jude’s team of researchers who battle much tougher obstacles on a daily basis in search of cures for some of the toughest cases of cancer and other catastrophic childhood diseases. Vynckier raised $470 to contribute to these efforts.

Vynckier Enclosure Systems participating teammates included:

  • Aaron Banks
  • Natalie Hart
  • George King
  • Myrna King
  • Monty Ortiz
  • Janet Tillmans

The Dash comes to Galveston every year, so keep an eye on www.beachdash.com for future dates and join Vynckier in the fun next time!